Narrow By
  1. Your SelectionAll

Service Support - FAQs

FAQ Search
Most Recently Published FAQs

Results 71 - 80 of 100

FAQ ID Description
FA105590Are the ATS46D17N, ATS46D22N, ATS46D32N, ATS46D38N, ATS46D47N, ATS46D62N, ATS46D75N, ATS46D88N, ATS46C11N or ATS46C14N repaired in the field or is it sent to the depot for repair?
This unit normally goes in for repair to the depot for warranty work.However, if this unit is part of an enclosed soft starter package (8636, 8638...
FA105545Who provides support for the 8808 Econopak Wound Rotor Controllers?
This device was a variable speed controller used on wound rotor motors from 50 to 2250hp and 240 to 4160vac. A small fixed resistance was installed...
FA104919Customer has an HVL/cc switch and the operating handle socket is wearing out. Can he replace the socket for the handle?
Customer has an HVL/cc switch and the operating handle socket is wearing out. Customer was operating this switch 900 times per year for 3 years....
FA104736How can one schedule FSD for startup of a drive?
To schedule FSD for the startup of a drive can go directly through the associated Field Service Office to coordinate time for visit. CTA-ID : 2010939...
FA104307Do we offer Multilink planning services, cost analysis, recommend installers etc.?
No, Refer to the local field office CTA-ID : 2010092
FA103244Where does the customer get a hard copy of an extended warranty purchased for an Altivar ATV66 with a paid startup?
This is handled through field services and should be documented in the qoute to cash number it was purchased on.Extended warranty is purchased when...
FA101461Who provides support for Class 6522 Bubbler / LevelPak or 6524 Programmer devices.
These devices were used to monitor and control the fluid level and pump sequencing in a process. The programmer would monitor the actual level, compare...
FA101393Who provides support for Class 9050 Type F Fiber Optic control products?
The class 9050 Fiber Optic System was used in Division 1 Hazardous locations as an alternative to traditional electrical controls. The network consisted...
FA101395Who provides support for Class 9043 Type AG Solenoid Valve products?
These devices were obsoleted several years ago, with no replacement. Telemecanique does not offer a solenoid valve for sale in the United States....
FA101394Who provides support for Class 9045 Type BG Magnetic Unloader products?
The 9045 BG Magnetic unloaders were electrically activated relief valves used to relieve head pressure on compressors. These devices have been obsolete...

Results 71 - 80 of 100