Narrow By
  1. Your SelectionAll

Product Features - FAQs

FAQ Search
Most Recently Published FAQs

Results 31 - 40 of 100

FAQ ID Description
FA168123ATV61HD....N4D: Is a line reactor required if the DC choke is not used?
Yes.  If the DC choke is not used, a 5% line reactor must be installed on the line side of the VFD. This applies to ATV61/71 sizes: 125 HP 460V and...
FA168153Are the ATV61/71 high horsepower drives available without the DC choke?
Yes.  Add a D suffix to the drive part number. For example: ATV61HC22N4 includes a DC choke. ATV61HC22N4D does not include a DC choke. CTA-ID :...
FA168169How can firmware be upgraded on ATV61 or ATV71 drive?
Need to send the drive back to repair depot to get Firmware flashed or get a new control board with the latest firmware. CTA-ID : 2062962
FA168168What is the EZM3EXT6?
The EZM3EXT6 is a 6 inch wide, 3phase-4wire bus extension piece used ONLY for EZM metering. CTA-ID : 2062960
FA168172What is the part number for lugs for a CK circuit breaker?
The CK circuit breaker, as well as the lugs, are obsolete. Contact us at 888-778-2733 to discuss a replacement. CTA-ID : 2062957
FA168154When replacing the Graphic keypad, VW3A1101, on an ATV drive, is any programming required?
No.  The program file resides in the drive.  When used with ATV61/71, there is the option to save the file to the keypad. CTA-ID : 2062757
FA168138On the ATV61/71, can FORWARD and REVERSE logic inputs be switched while the drive is running?
Yes.  When the direction is switched, the drive will ramp to a stop and then ramp up to the speed reference in the opposite direction. CTA-ID :...
FA168173An ATS48 soft starter with remote keypad will allow access to only the status and SUP menu.
On the back of the remote keypad, there is a 3 position switch.  If this switch is in the ``FULLY LOCKED`` position, it will not allow access to any...
FA168174How is the ATV212 set up for a run permissive logic input?
Wire a dry contact to P24 and a logic input (F, R, or RES).  Program F110 = 0 to remove the always active run permissive.  Then set the logic input...
FA168158What is the power supply voltage specification for the ATV312?
Voltage ranges are as follows: 200 - 15% to 240 + 10% for models ATV312....M2 200 - 15% to 240 + 10% for models ATV312....M3 380 - 15% to 500 + 10%...

Results 31 - 40 of 100