Narrow By
  1. Your SelectionAll

Codes/Std/Certification - FAQs

FAQ Search
Most Recently Published FAQs

Results 71 - 80 of 100

FAQ ID Description
FA109027Are the IEC K-Line contactors SEMI F47 compliant?
K-Line contactors are SEMI F47 compliant. Additionally, the addition of an overload relay makes them SEMI F47 compliant motor starters.The K-Line...
FA99869Do Square D`s 9070 industrial control transformers (CPT) conform to the new IEC standard EN61558-1?
Yes, Square Ds 9070 CPTs do conform to EN61558-1.  To view the certification on-line, go to the CEDocumentation portion of Square D`s intranet and...
FA101390Are Square D instrument (current and potential) transformers listed for UL and cUL (CSA)?
Most instrument transformers listed in Square Ds Instrument Transformer catalog, document #4210CT9701R6/01, are UL and cUL Recognized per Classification...
FA102173Do the transformers offered in Square D`s Hospital Isolated Power Systems meet the UL standard 2601 for ``medical grade transformers``?
Square D does not offer any transformers to meet UL 2601.However, Square D`s Hospital Isolated Power Systems are built to UL standards 1022, and 1047....
FA99192What is NEMA KS1 as it refers to enclosure types?
NEMA KS1 is in reference to the NEMA standard that addresses the manufacturing of safety switches. It is not an enclosure type, although enclosure...
FA90082Will the Altivar ATV56 drive meet the IEEE 519 standard of recommended practices and requirements for harmonic control in electrical power systems.?
The IEEE 519 is a system standard not a component standard. All power system impedences must be considered to meet this standard including transformers,...
FA144769What is a CAGE code?
It is a Commercial and Government Entity code. Contact Tonya Blum at extension 56251 or Nona Wagner-Babischkin at 410-847-1306. CTA-ID : 2059749
FA144770Is a Material Safety Data Sheet (MSDS) available for PK49SP touch-up spray paint?
Use the internet address below to download a copy from our Technical Library: http://static.schneider-electric.us/docs/Electrical%20Distribution/Safety%20Switches/PK49SP%20Material%20Safety%20Data%20Sheet.pdf CTA-ID...
FA144474Is the EV230WSRR UL Listed?
Yes, it is. The UL File is #E338176. CTA-ID : 2059790
FA144520What is the NEMA rating or IP degree of protection for the door-mounted 32598 RE12 and 32600 RE22 rotary handle operator for the Powerpact D frame (and NSJ) breaker?
32598 and 32600 are IEC-Style Door-Mounted Rotary Operating Handles.  The handle mechanism can be used in NEMA 3R and 12 enclosure applications. ...

Results 71 - 80 of 100