| FAQ ID |
Description |
| FA126996 | Is the 82455 UL listed? Yes, this device is UL listed and is labeled cULus, File E-2875. CTA-ID : 2048606 | | FA126574 | Is the H82355 UL listed? Yes, this device is UL listed and is labeled cULus, File E-2875. CTA-ID : 2048605 | | FA126679 | Is the 82355R UL listed? Yes, this device is UL listed and is labeled cULus, File E-2875. CTA-ID : 2048604 | | FA126680 | Is the 82345 UL listed? Yes, this device is UL listed and is labeled cULus, File E-2875. CTA-ID : 2048609 | | FA126575 | Is the H82455 UL listed? Yes, this device is UL listed and is labeled cULus, File E-2875. CTA-ID : 2048608 | | FA126678 | Is the 82355 UL listed? Yes, this device is UL listed and is labeled cULus, File E-2875. CTA-ID : 2048603 | | FA126677 | Is the H82255 UL listed? Yes, this device is UL listed and is labeled cULus, File E-2875. CTA-ID : 2048601 | | FA126790 | Is the 82255R UL listed? Yes, this device is UL listed and is labeled cULus, File E-2875. CTA-ID : 2048600 | | FA120915 | Is the 82345R UL listed? Yes, this device is UL listed and is labeled cULus, File E-2875. CTA-ID : 2034733 | | FA116411 | Are the GV2 IEC manual starters CE compliant?
Note: This applies to all GV2L__, GV2LE__, GV2M__, GV2ME__, GV2P__, GV3M__, GV3ME__, GV7RE__ & GV7RS__ manual starters. These manual starters are manufactured in Europe and do meet the CE Directive. CE Declaration of Conformity is available through the attached web... |
|