| FA91100 | Does the Altivar 58 unit have Auto-Manual switching? Yes, the unit does have Auto/Manual switching.The function is used to switch between two different analog input signals for the speed reference.The... |
| FA104083 | How can run status output be derived from an Altivar 58 drive? The R2 relay can be programmed for run status. The R2A and R2C contacts will close when there is a valid run command.Unlock the keypad. Remove all... |
| FA92877 | Why does Altivar ATV58 with a General Purpose Option card not retain the settings? The GPO card settings are not immediately saved when a user pressed the enter key. Upon final programming of the option card users must go to Menu... |
| FA105357 | Why does the Altivar 58 display not allow changes to a parameter from unknown assignment? This is likely because the keypad revision is not the same as the revision level for the control board.Keypad replacement may be necessary. The keypad... |
| FA115824 | How can an emergency stop be connected to the Altivar 58? A true emergency stop should not rely totally on the drive to interrupt power to a motor. Consider the use of power interrupting devices such as shunt... |
| FA117053 | Is the Frequency Reference for keypad command with the ATV58 retained on loss of power? On loss of power the local speed reference (Frh or LFr) goes back to the Low Speed setting (LSP).The last reference will be lost. CTA-ID : 6827 |
| FA108472 | What functions are available for the R2 relay on the ATV58? The R2A is a N/O pogrammable relay.The relay can be assigned to: no: not assigned FtA: frequency threshold attained. The contact is closed when... |
| FA106346 | How can the frequency for the ATV58 unit to run above 60hz? The high speed (HSP) can not be set higher than the Maximum Frequency (tFr).tFr is in the drC menu. Increase this value to about 20% greater than... |
| FA115571 | How can external contacts be used to stop the Altivar 58? There are multiple ways to stop the ATV58 drive. The stop method used depends on how the drive is being controlled. It is very important to configure... |
| FA103423 | How is PI control enabled in the ATV58 for setpoint control? Set AI2 in menu 5 (I/O menu) for PIF.This function is available after enabling the Variable torque Macro and ensuring that the Auto/man (RFC) parameter... |