| FA164703 | On an ATS48, how is the R1 relay set to control an isolation contactor? From the display status screen, typically rdY or nLP, arrow down to the IO menu and ENT. Arrow to parameter r1, ENT and change to R1I. ENT to save.
CTA-ID... |
| FA164712 | How is auto fault reset configured on the ATV212 or S-Flex 212 drive? Set F303 to anything other than 0. The value will indicate the number of fault reset attempts to be made before the drive requires a manual reset.
CTA-ID... |
| FA164350 | How can you set up the ATV32 drives to utilize the multipoint configuration with one HMI?
You must assign each ATV32 drives modbus address between 1 thru 247.
Goto: FULL menu
Goto: CON menu
Goto: nd1 menu
Add= Modbus address
tbr= Modbus... |
| FA164558 | How is an ATV212 reset to factory defaults? Set tYP = 3 to return to factory settings (remember to press and hold enter for 2 seconds). Then set tYP = 2 to configure for 60Hz .
CTA-ID :... |
| FA164561 | How do you turn off the torque control in the ATS22 softstarts? Under the ConF menu scroll to parameter LAC, push the ENT button. Change from oFF to On. Push ENT button to save.
Next, go to the AdJ menu and... |
| FA164107 | Will the remote VW3A1101 HMI have speed control over the drive if FNOD is set to 3? Yes the HMI`s wheel will have speed control over the drive.
CTA-ID : 2061155 |
| FA163780 | How do you wire a external 24vdc digital output from a PLC to the input of the ATV21 or 212 drive?
Make sure the Source, CLP, Sink dip swtich is set to CLP.
Example of PLC with a sourcing output.
ON the ATV21 or ATV212 drive jumper PLC and CC... |
| FA163613 | How do you setup Metasys N2 on the ATV212 Drives?
Controlling Drive with N2 with start stop and speed reference.
FNOD= 4
CNOD= 2
F108 is 0
F807 =1 terminal wiring or 0 for RJ45
F829= 2 N2... |
| FA163611 | Can you do a multipoint addressing with the ATV312 drives?
It is not possible to do multipoint addressing with the ATV312 drives. The menu for the configuration can be displayed on the remote HMI but... |
| FA162478 | How do you setup the ATV21 and ATV212 drives for Modbus?
Monitor only set up example
CNOD=0 terminal control
FNOD= 2 for VIB
THr = FLA of motor name plate
F---- enter
F108= 48 Force to local mode... |