| FA166279 | How is the DC injection braking setup on the ATV212 drives? Program the following:
F250 = DC braking starting frequency, set to a value > 0
F251 = DC braking current level
F252 = DC braking time
Caution:... |
| FA166256 | How is the ATV212 setup for 2 preset speeds? The slower speed is assigned to LL and a logic input activates the higher speed which is assigned to Sr1.
For example, logic input R is assigned... |
| FA164739 | How do you wire up a 24vdc push pull encoder to the VW3A3407 encoder option card for the ATV71 drive? The pin outs may vary depending on the encoder type and connector type.
Basic setup is as follows:
A from the encoder goes to A on the encoder card
B... |
| FA166177 | VW3A8114 modbus bluetooth adaptor configuration set up. Bluetooth connection
1. Connect a Bluetooth adapter to your computer and the drive.
2. From your control panel
2.1 Click on “Bluetooth... |
| FA165515 | ATV71 how can your program the normally closed contact on the R1 relay (terminals R1C to R1B) for a run status? By default on the ATV71 drives, R2 is configured as a Drive Run contact. To change R1 to Drive running:
Go into Main Menu > Drive Menu > 1.5 Inputs/Outputs... |
| FA165567 | How is the maximum speed changed in the ATV31 or ATV312 drive so that the motor can operate above 60Hz? Parameter HSP determines the maximum speed the drive can operate. Parameter tFr determines the maximum value that HSP can be adjusted.
By default,... |
| FA165576 | What software is used to program the Controller Inside Card? Codesys is the software is used to program the Controller Inside Card. This software is only available after completing the training class for this... |
| FA89006 | Can the Omegapak 8804 PT frequency be increased above 60 hz? R86 is a snip out resistor. With this removed, the max speed will go up to 90 hz. Adjust the high speed with potentiometer P3. CTA-ID : 4210 |
| FA165413 | ATV12 and ATV32 firmware update instructions. To update the ATV12 or the ATV32 firmware revision you will need a VW3A8121 Multiloader and a VW3A8122 cable.
See the attached file for instructions. |
| FA165168 | How can I set an ATV61 or ATV71 for HMI speed reference and terminals for start/ stop controls? 1.6 Command menu
Set ref ch 1 to HMI
Set Profile to separate
CMD switching =channel 1 active
CMD channel = Terminal control
1.7 Application Function... |