| FA166888 | ATS22 soft start is tripping on SnbF and this code cannot be cleared. SnbF indicates that too many starts were attempted based on the settings for parameters Snb (number of starts) and SLG (starts period). The soft... |
| FA97528 | Can the In Phase Loss on the 8803 Omegapak be turned off? This can only be done on the CT style units and is changed using the Commissioning terminal (8803 PPO1 ) or PC software (no part number). Go to the... |
| FA166691 | How is the ATS22 set for 3 wire control? Wire the momentary normally closed STOP contact to LI1 and the momentary normally open START contact to LI2.
Program the ATS22. In the I-O menu,... |
| FA166743 | How can the ATV61 drive be prevented from going into reverse when the HMI dial is turned to the negative range? In Menu 1.6 COMMAND, set RV Inhibition to Yes. This also applies to the ATV71 drives.
Note that this does not prevent reverse operation when the... |
| FA166718 | How can frequencies be skipped in an ATV61 / ATV71 ? In menu 1.3 Settings, adjust the following parameters:
Skip Freq = desired frequency ( in the middle of the skip range )
Skip Freq Hysteresis = (+)... |
| FA166704 | How do I assign the analog output to show motor power on an ATV312 drive? Program the following parameter codes
Inputs and Outputs menu:
CODE SET DESCRIPTION
AO1T v or I Configuration of AO1t=0A,... |
| FA166713 | How do I change the profibus address on the ATV61 or ATV71 with an optional profibus card? Profibus card part numbers are VW3A3307 or VW3A3307S371.
The profibus address is set through a series of 8 dip switchs on the card beside the 9... |
| FA166708 | On an ATV212, what parameter sets the drive for a 0-10Vdc analog input reference on VIB-CC? Set FNOd = 2 and wire your 0-10vdc signal to VIB and CC.
CTA-ID : 2062125 |
| FA166750 | On the ATV21 and ATV212 Drives, what parameter determines the allowed motor rotation direction? Parameter F311 is the motor rotation direction command.
F311 = 0 is FWD and REV operation is permitted
F311 = 1 is FWD operation only factory default)
F311... |
| FA166717 | On an ATV21 or ATV212, how is the high speed increased to a value greater than 60Hz? First set the maximum frequency, FH, to at least the desired high speed.
Second, change the high speed, UL, to the desired value.
CTA-ID : 2062050 |