| FA128147 | Are the ATV21 and ATV212 drives plenum rated? The open type ATV21/ATV212 and the enclosed SFLEX are plenum rated. The SFLEX is stated in the brochure (8839BR0501R8/07) under environmental specs... |
| FA170355 | What is the case material for the Powerpact P breaker? The case material is R/C polyester plastic (QMFZ2), ref. CIC 25630 mfg. by Menzolit
CTA-ID : 2063143 |
| FA130527 | Can the ATV12 keypad be used with the ATV312 or ATV32 drives? Yes, plus you need to order either the 1 or 3 meter ATV61/71 cable to use with it. CTA-ID : 2054051 |
| FA169529 | Can the NEMA Class 8502 contactor be converted to a Class 8536 starter by installing an overload relay? The NEMA size 00, 0 & 1 contactors can be converted to starters by ordering and installing the appropriate replacement overload relay. However, due... |
| FA109953 | Is the 9 volt dc battery adapter available for the Class 9065 Type SP__ Motor Logic Plus solid state overload relay?
This part is provided with each overload relay but is not available as a separate item.CTA-ID : 2019075 |
| FA169368 | What is the difference between a GV2P20H7 and GV2P20? In the United States, only the `H7` version is used. The device label will have details that only apply to North America. The `H7` is not referenced... |
| FA169363 | What is the difference between a 2510KO2C and 2510KO6C non-reversing starter? The 2510KO2C has a 2HP@115VAC - 7.5HP@230VAC - 10HP@460/575VAC horsepower rating at 3 phase
The 2510KO6C has a 2HP@115VAC - 7.5HP@230VAC - 15HP@460VAC... |
| FA169359 | What exactly is a combination arc fault circuit interrupter or CAFI breaker? A combination arc fault circuit interrupter combines branch/feeder protection with outlet circuit protection.
The branch/feeder AFI breakers only... |
| FA168589 | The test button on a QO-GFI or HOM-GFI breaker will not trip the breaker; is the breaker bad? First ensure that the breaker is properly installed in an energized panel with the pigtail connected to the neutral bar.
If the breaker will not... |
| FA168588 | Does the new CAFI breaker have more arc-fault detection capabilities than the previous AFI breaker ? Yes, the CAFI breaker detects both series and parallel arcing. The AFI breaker detects parallel arcing only.
CTA-ID : 2063067 |