Narrow By
  1. Your SelectionAll

Wiring - FAQs

FAQ Search
Most Recently Published FAQs

Results 91 - 100 of 100

FAQ ID Description
FA128201Does the jumper on T1 and T2 on the terminal strip of a PGL breaker need to be removed if wired with a neutral CT?
Yes. Remove and discard the shorting jumper from T1 and T2, if a CT is installed. The installation guide for that trip unit is: 48041-082-03.CTA-ID...
FA128150What is the Square D part number for a lug equivalent to Ilsco D3121 or CMC LA750-2
Use Square part number 40251-136-50.CTA-ID : 2050012
FA128027Can the TVS120XR40S be wired to operate on a 120V 2 wire + G system?
Yes. To make it work connect both black wires of the TVSS to the phase wire to make it work. However, we recommend the TVS120XRS for this application.CTA-ID...
FA127881What are the terminal numbers to connect an undervoltage trip coil on an H or J frame circuit breaker?
Constant voltage at the correct level for the device (24V, 120V, AC, DC, etc) should be applied to terminals numbered D1 and D4. Designation for...
FA127847What is the lug size on a HU363DSWC and are there double lugs for it?
The lug takes (1) # 12 - # 1/0 (Al) or (1) # 14 - # 1/0 (Cu). There are no double lugs available for this switch. CTA-ID : 2050310
FA127833Is it permissible to have parallel circuits being fed from the QO120AFI Arc-D-tect breaker?
No. The QO-AFI breakers are not intended for parallel or multiple circuits.CTA-ID : 2050270
FA127807Can the 9001BW256 (ON-OFF Maintained) or any of the devices using contact symbol #10 be wired for a two wire control circuit?
Yes, just wire to the N.O. ON contact. When it is pushed it will close and remain closed until the OFF button is pushed when it will then open. (The...
FA127688Can GV2, GV3 and GV7 starters be backfed ?
Not recommended.CTA-ID : 2049249
FA127241How do you wire the shunt trip on a EDB34020SA breaker?
Wire the switched hot 120 V wire to terminal 7 and the neutral to terminal 6.CTA-ID : 2049413
FA127226What is the acceptable wire size for a QOB-VH, 3 pole breaker 40 amp through 70 amp?
These breakers will accept a #8 - #2 Cu/Al wire.CTA-ID : 2049025

Results 91 - 100 of 100