Narrow By
  1. Your SelectionAll

Wiring - FAQs

FAQ Search
Most Recently Published FAQs

Results 71 - 80 of 100

FAQ ID Description
FA130949Will a PK23GTA Equipment Ground Bar accept either solid or stranded conductors?
Yes, this ground bar will accept either solid and stranded wire. However, there is an exception if terminating two ground conductors of different...
FA130957Will a PK15GTA Equipment Ground Bar accept either solid or stranded conductors?
Yes, this ground bar will accept either solid and stranded wire. However, there is an exception if terminating two ground conductors of different...
FA130950Will a PK27GTA Equipment Ground Bar accept either solid or stranded conductors?
Yes, this ground bar will accept either solid and stranded wire. However, there is an exception if terminating two ground conductors of different...
FA130952Will a PK15GTA-FT Equipment Ground Bar accept either solid or stranded conductors?
Yes, this ground bar will accept either solid and stranded wire. However, there is an exception if terminating two ground conductors of different...
FA130911Will a PK23GTA-L Equipment Ground Bar accept either solid or stranded conductors?
Yes, this ground bar will accept either solid and stranded wire. However, there is an exception if terminating two ground conductors of different...
FA130651Is there a double barrel lug available for the HU364RB, Series F Heavy Duty Safety Switch?
Yes, order a AL20DTF which contains (3) lugs per kit, that will accept (2) #6 AWG - 300 KCMIL. Two kits are required to modify both the line side...
FA130455What size cable does a LAD7B10 accept?
It takes either a 1 flexible cable without cable end size 14-8 AWG or 1 flex cable with cable end size 16-12AWG or 1 solid cable without cable end...
FA129920On a SDSB1175C surge suppression unit what size breaker do we recommend?
To protect an SDSB1175C, the application must use a 15-30 ampere rated breaker, because the connecting wire must be also protected. CTA-ID : 2053054
FA129810What is the Terminal Lug Data for a H361DS, Series F06 (F6) Heavy Duty safety switch?
The lugs on this device will accept (1) #12 - 2 AWG aluminum or (1) #14 - 2 AWG copper conductors per phase OR (2) #14 - #10 Copper (solid or stranded)...
FA129632What is the Terminal Lug Data for a H361AWK, Series F06 (F6) Heavy Duty safety switch?
The lugs on this device will accept (1) #12 - 2 AWG aluminum or (1) #14 - 2 AWG copper conductors per phase OR (2) #14 - #10 Copper (solid or stranded)...

Results 71 - 80 of 100