| FA109517 | Is a line isolation contactor or shunt trip circuit breaker needed with SquareD soft starters? Since the solid-state switches may be incapable of completely blocking the motor power should a fault occur, auxiliary isolation on the line side... |
| FA108350 | Where can a customer find the wiring diagram or schematic for the U-Line Motor Starters? In the U-line catalog, 8502CT0201. CTA-ID : 2015240 |
| FA110634 | Can the ATS01 soft starters be wired inside Delta? Yes. This is true of the entire range of ATS01 products.If help is needed, record the nameplate data from the soft starter and contact technical support... |
| FA101945 | Does Square D offer a lug kit for any of the encapsulated transformers? Most of the the encapsulated transformers that Square D offers are cable leaded units. As such, Square D does not offer connectors for cable-to-cable.... |
| FA98600 | What is pin out of Digital Operator Interface card for the Omegapak 8804? Wiring diagrams for the DOI manual start on page 65 of 50006-377-02. CTA-ID : 4132 |
| FA112821 | Does it matter where the pull up / pull down resistors are located within the ATV31 multiple drive network? Not really.The ATV31 does not have internal pull up / down resistors for the rs-485 communications. Therefore, if it is used on a network with PLC... |
| FA101539 | Why does the ATS48 unit not start and it does not indicate that have a fault, have adequate control power on CL1 and CL2 as well as have closed 24v to the run terminal. In order for the ATS48 to receive a run command and start it not only has to have 24v to run terminal, but it also has to have 24v to the stop terminal.... |
| FA109874 | What would cause the ATV58 , EconoFlex drive to not follow the 0-10 volt signal? The drive must have MOD J09. This includes a signal converter circuit that connects to the control terminals of the drive power converter control... |
| FA101144 | What are the MICROLOGIC Series B Ground Fault Alarm signal terminals? Terminals A, B on the wiring diagram correspond to the following breaker terminals:LE, ME, NE, PE: 8,9SE: 21, 22Terminals for 120 Vac GF push... |
| FA96087 | Can multiple motor leads fed from AC Drives share a conduit or raceway? It is not recommended that output cables from different AC drives share close proximity in raceways or conduits. Because of the high frequency switching... |