| FA166736 | How is a potentiometer connected for speed reference to a ATV212? Connect the pot wires to terminals PP (+10V) , CC (com) and VIB (analog input).
CTA-ID : 2062038 |
| FA91357 | How does start/stop control wire on the 8660 SSRVS old style unit? A Stop pushbutton is wired between terminals 1 and 2, a Start pushbutton is wired between terminals 2 and 3. Must supply 115 volts ac on terminals... |
| FA165552 | Can the ATV312 with 3-phase input be powered up with 120 Vac, single phase for programming only? If the ATV312 is rated for 230 Vac input you may be able to program with 120V supply power. For the 480V and 575V rated drives, 120VAC is too low... |
| FA165571 | How long can the motor leads be on a ATV212 S-flex drive? The longer the cable, the greater the capacitance. Cable lengths greater than 164 ft (50 m) may appear as a ground fault condition to the drive. For... |
| FA165551 | What is the fault code PRA on ATV61 or ATV71 drives? PRA is a drive state meaning power removal function active. The drive is not seeing 24VDC on the terminals between PWR and +24. Confirm that the... |
| FA162187 | What is the terminal lug data for the HU266R heavy duty safety switch? The HU266R will accept (2) 3/0 to 750kcmil (Al/Cu) wires per phase and neutral.
CTA-ID : 2060911 |
| FA162005 | What cable is required for the Powerpact H, J and L ENCT? Connecting Cable: Belden 9451SB 22 AWG (0.32 mm2)
stranded, shielded cable
CTA-ID : 2060716 |
| FA115085 | How can an ATS48 be wired for 3-wire control? Wire a normally closed stop pushbutton between the +24 and STOP terminals.Wire a normally open start pushbutton between the +24 and RUN terminals.If... |
| FA87946 | Why does the drive output frequency not increase to the desired speed reference using 0-10 VDC control to AI1 for the Altivar FVC drive? AI1A and AI1B are bipolar inputs. When not using bipolar speed reference it is necessary to jumper AI1B to common. See the attached Installation Guide... |
| FA97759 | When replacing a medical digital clock/timer MCT-12B with a new MCT-12B that is to be connected to an existing MCT-BP battery back-up, the orginal MCT-12B had a gray cable that was hardwired into it that was then wired to the bottom of the MCT-BP battery back-up. Can this existing cable be used with the new MCT-12B? Yes, the existing cable can be re-utilized to connect the new MCT-12B to the existing MCT-BP. CTA-ID : 12954 |