| FA168587 | What are the pinouts for the Micrologic trip unit Breaker comms module (BCM)? From left to right:
E1: 24Vdc
E2: GND
E3: Out- Black
E4 Out+ Red
E5: In- White
E6: In+ Green
This applies to Powerpact P, R and Masterpact NW,... |
| FA167981 | ATV312 tripping on ObF fault. If the drive trips while running, then check for power surges or spikes. Need to monitor for voltage surges and spikes. May need to install a line... |
| FA167398 | ATS01N212RT: The customer cannot get the soft start to run the motor. The ATS01N2**LU/QN/RT models require a run command on the control circuit.
A START/STOP contact can be wired to LI+ and LI2. This will allow soft... |
| FA166884 | How is a start command given to an ATS48? The ATS48 can start with either 2 wire or 3 wire control.
For 2 wire control: Wire a jumper between the STOP and RUN terminals. Close a dry contact... |
| FA88143 | Where would you put a 4-20 signal for speed reference instead of using a 0-10v on an Omegapak 8803? Need to connect the milliamp signal between OE1 (common) and EC. CTA-ID : 4042 |
| FA166828 | How can ATS01N2...LU, QN, RT be started without control wires? Add a jumper between terminals LI+ and LI2. This provides a continuous RUN command. When power is supplied to the ATS01, it will immediately begin... |
| FA92390 | Where do you wire the speed potentiometer on the Omegapak 8803 Type P unit? The Speed pot is wired on terminals OE1, E1, P10 . The wiper goes to E1 terminal, P10 is the +10v and OE1 is com (0v). CTA-ID : 4045 |
| FA91123 | Why does the speed potentiometer adjust speed in hand and auto for this 8804 Omegapak? With the E07 option card, if terminal 16 is tied to 78 the drive will use the POT for speed in hand and auto.Remove this jumper to allow a separate... |
| FA166744 | HCR548612U: what is the wire size for the incoming conductors? The lugs are rated for 4 - 3/0 thru 750kcmil cables but the UL wire bending range for the interior and box limits cable to 4-3/0 thru 500kcmil
CTA-ID... |
| FA166719 | How do I start and stop the motor on the SFlex 212 drive through the field terminals? This can be accomplished by closing and opening a dry contact connected between the field terminals P24 and F.
CNOD=0 and you will need a speed reference.... |