Narrow By
  1. Your SelectionAll

Wiring - FAQs

FAQ Search
Most Recently Published FAQs

Results 1 - 10 of 100

FAQ ID Description
FA168587What are the pinouts for the Micrologic trip unit Breaker comms module (BCM)?
From left to right: E1: 24Vdc E2:  GND E3: Out-  Black E4 Out+  Red E5: In-   White E6: In+  Green This applies to Powerpact P, R and Masterpact NW,...
FA167981ATV312 tripping on ObF fault.
If the drive trips while running, then check for power surges or spikes. Need to monitor for voltage surges and spikes. May need to install a line...
FA167398ATS01N212RT: The customer cannot get the soft start to run the motor.
The ATS01N2**LU/QN/RT models require a run command on the control circuit.   A START/STOP contact can be wired to LI+ and LI2. This will allow soft...
FA166884How is a start command given to an ATS48?
The ATS48 can start with either 2 wire or 3 wire control. For 2 wire control: Wire a jumper between the STOP and RUN terminals.  Close a dry contact...
FA88143Where would you put a 4-20 signal for speed reference instead of using a 0-10v on an Omegapak 8803?
Need to connect the milliamp signal between OE1 (common) and EC. CTA-ID : 4042
FA166828How can ATS01N2...LU, QN, RT be started without control wires?
Add a jumper between terminals LI+ and LI2.  This provides a continuous RUN command.  When power is supplied to the ATS01, it will immediately begin...
FA92390Where do you wire the speed potentiometer on the Omegapak 8803 Type P unit?
The Speed pot is wired on terminals OE1, E1, P10 . The wiper goes to E1 terminal, P10 is the +10v and OE1 is com (0v). CTA-ID : 4045
FA91123Why does the speed potentiometer adjust speed in hand and auto for this 8804 Omegapak?
With the E07 option card, if terminal 16 is tied to 78 the drive will use the POT for speed in hand and auto.Remove this jumper to allow a separate...
FA166744HCR548612U: what is the wire size for the incoming conductors?
The lugs are rated for 4 - 3/0 thru 750kcmil cables but the UL wire bending range for the interior and box limits cable to 4-3/0 thru 500kcmil CTA-ID...
FA166719How do I start and stop the motor on the SFlex 212 drive through the field terminals?
This can be accomplished by closing and opening a dry contact connected between the field terminals P24 and F. CNOD=0 and you will need a speed reference....

Results 1 - 10 of 100