| FA88595 | What are the repair parts for a HOM20M100RB, Series S01 load center? Only the parts listed below are considered field replaceable.Cover - 4054802209Cover Mounting Screw - 2142717161 (2 Required)Interior Trim - 4056513401... |
| FA127919 | What are the rating plug part numbers for the CK800 Circuit Breaker? The CK800 circuit breaker, as well as the rating plugs, are obsolete. Contact us at 888-778-2733 to discuss a replacement.As a reference, here are... |
| FA90963 | What are the rating plug part numbers for the CK400 Circuit Breaker? The CK400 circuit breaker, as well as the rating plugs, are obsolete. Contact us at 888-778-2733 to discuss a replacement.As a reference, here are... |
| FA121960 | What are the catalog numbers for the field-installable undervoltage shunt trip accessories for Powerpact DG, DJ, and DL type circuit breakers? The field-installable shunt trip devices are as follows:Volts AC Suffix Cat. # 24 SK S29384 48 SL ... |
| FA90931 | What is the part number for a replacement load base assembly for a D325N General Duty safety switch? The part number will depend on the Series number of the safety switch. For a Series E3, use 4051062850,. For Series E2 or E1, use 4051046550. For... |
| FA124809 | What is the replacement for the Q22200P breaker?
The replacement breaker is obsolete, no longer available with no replacement.Q22200P was a special 200A 2P Q2 breaker built for HITCH-N-POST METER... |
| FA167440 | What is the difference between the ET1.0I and Micrologic trip units? ET1.0I is a fixed amperage non interchangeable trip unit. Has instantaneous adjustments.
The Powerpact P, R and Masterpact Micrologic is an adjustable... |
| FA104853 | Can breakers with suffix AFI, CAFI, GFI, or EPD be used on a 2-wire 120V ungrounded system? No, the these breakers can only be used on solidly grounded systems. CTA-ID : 2011220 |
| FA167397 | Why does the ATS22 soft starter cost less than the ATS48, when the ATS22 has an internal shorting contactor? The ATS48 is a more robust soft starter that can handle a wide range of applications. A shorting contactor is recommended for all applications.
The... |
| FA167396 | Does the HL100WN2M16 come with the steel roller lever arm? No the steel roller lever arm must be purchased separately. The body is machined aluminum, the roller itself is steel.
We offer different lengths... |