| FA167450 | Can we get a 3/4`` hub in a 9001BR station? No, only the 1/2 inch NPT is available.
CTA-ID : 2062176 |
| FA167446 | ATV312: What is the COS parameter? This is the Power Factor Parameter, located in the drC menu.
Look at the motor nameplate and use the power factor, typically designated as PF or... |
| FA167441 | Will the HMI part number VW3A28101 work with a ATV312 drive ? No. This is not a valid configuration.
CTA-ID : 2062168 |
| FA119519 | How many spaces will a CAFI breaker take? Both QO and Homeline CAFI circuit breakers take one pole space. CTA-ID : 2031815 |
| FA167413 | What is the command word for the ATS22 soft starters?
The command word address for the ATS22 soft starter is 752.
The ETA status word address for the ATS22 soft stater is 256
See the attached PDF document... |
| FA167391 | Will two single-pole QO breakers mount in QO2100BNF? No, this enclosure is not for use with one-pole QO circuit breakers.
CTA-ID : 2062540 |
| FA167395 | An ATS22 display is showing OHF (Over Heating Fault), but the starter has not been run for several hours and the ambient condition is very cold. The low end operating temperature for the ATS22 is 14 degrees F. Below this, the starter will fault and show OHF. OHF is an indication that the... |
| FA167389 | Does 9007CR53B2 include the 9007B head? Yes, it does.
CTA-ID : 2062486 |
| FA167392 | What load centers use the PK2MB Retaining hold down kit? The PK2MB Retaining hold down kit is designed for use ONLY in the QO612L100F/S/RB/DF/DS, QO816L100F/S/RB/DF/DS and QO148L125GF/S/RB load centers.... |
| FA167394 | What is the prefix H on the HL100WN2M16? The prefix H is for high temperature 0 to +350 degree F, and requires the use of the metal front cover .
The minimum temperature 0 degrees F is based... |