| FA167798 | With an ATV212, is there a auto/ manual configuration to switch between PID reference and a second analog reference? [Auto/man speed ref] Auto/Manual Speed Reference Switching 0
0 [Enable]
1 [Disable]
Switching between two speed reference sources by means of a logic... |
| FA167797 | Can I run an ATS softstarter without a motor load or motor connection? It is not possible to run the ATS softstart unloaded. with no moto connected.
CTA-ID : 2062814 |
| FA167596 | Does the ATS22 soft start have an output relay for alarm? Yes. The standard unit has 2 relays ( R1 and R2 ) and either of these can be programmed for alarm.
CTA-ID : 2062693 |
| FA167436 | Can (2) MG26925 , 1a/1b aux contacts be used with a Multi 9 breaker Yes , there is provisions for stacking on the left side of the breaker up to 54mm (3`)
of accessories
CTA-ID : 2062625 |
| FA167438 | What is the wire range on a QOB2150VH or QOB3150VH breaker? Breaker will accept a single conductor #4-300 kcmil AL/Cu.
CTA-ID : 2062419 |
| FA167443 | What size threads are on the 9001R22? The 9001R22 has internal female threads 0.654-24.
CTA-ID : 2062512 |
| FA167451 | Do we offer 9001KN216 in plastic? No the 9001KN200 and 9001KN300 legends are only available in aluminum. This is because the lower half is so thin that it would break when it gets... |
| FA167447 | What are the components for the 9001KXREAAH12? Order the 9001KXREA A with (2) 9001KA2 contact blocks for position 1 and 3 and (2) 9001KA3 contact blocks for position 2 and 4.
CTA-ID : 2062214 |
| FA167442 | 9001OR120: What is the diameter of the mounting hole? 17.5mm or 0.68 inches.
CTA-ID : 2062381 |
| FA167445 | What is the XD2AC221? It is a 30mm joystick., a 2 direction with spring return to 0 with a 68mm long lever.
CTA-ID : 2062523 |