Narrow By
  1. Your SelectionAll

Product Features - FAQs

FAQ Search
Most Recently Published FAQs

Results 51 - 60 of 100

FAQ ID Description
FA168145On an E-Flex, what is modification B09?
This option provides a line contactor factory wired between the circuit breaker disconnect ( or line reactor when provided ) and the ATV61 power converter....
FA168120What type of enclosure is the MD3304X?
The enclosure is Non-metallic, rated for both indoor and outdoor use, is UV and corrosion resistant (Types 1, 3, 3R, 4, 4X, and 12). See the Instruction...
FA168118Are the Subway service fittings for the trench duct available?
No. The Subway product line and the service fittings are no longer available. Refer to page 14-1 of the Supplemental & Obsolescence Digest 174 for...
FA168126Is the LDGB wireway available?
No. LDB wireway is only available in a painted steel enclosure. CTA-ID : 2062909
FA168127Is the LDB wireway available in a galvanized housing?
No. LDB wireway is only available in a painted steel enclosure. CTA-ID : 2062908
FA91969Can voltage be continuously applied to shunt trip devices for Powerpact HD, HG, HJ, HL, and HR circuit breakers?
Yes, all Powerpact shunt trip accessories are continuous duty rated. CTA-ID : 2055503
FA110477What is wire range for the LAL tenant breaker used in the EZML111400?
The LAL tenant breaker will accept (1) #1 AWG to 600KCMIL or (2) #1 AWG to 250 KCMIL per phase as standard. CTA-ID : 2019901
FA118301What is the part number for the QMB circuit breaker adapter unit that accepts the Powerpact J frame breaker?
QMBJW.  Use a S37445 J frame breaker nut insert kit with this . CTA-ID : 2030443
FA167794How much smaller horsepower motor, can I put a ATV drive?
Rule of Thumb for smaller horsepower motors. The drive horsepower is higher than the motor horsepower. We recommend typically not going lower than...
FA167795ATV61 / 71 . Can I use a temperature sensor to control the drive speed?
No, the drive uses analog inputs. Temperature sensor output will need to be converted to voltage, current or a contact transistion (preset speed)...

Results 51 - 60 of 100