| FA168175 | On an ATV312, is drive protection compromised when OPL = NO? OPL is an output phase loss detection. This feature is intended to protect the motor from imbalanced current or single phasing. Disabling the feature... |
| FA168140 | On the ATV312, what type of connection accommodates the CANopen cable? The CANopen communication card has a port that accepts an RJ45 connector.
CTA-ID : 2062271 |
| FA168171 | How is a remote fault reset contact added to an ATV312? Wire the normally open reset contact to 24V - LIx. In the FLt menu, program rSF = LIx.
After the drive faults, a contact closure will reset the fault.
CTA-ID... |
| FA168177 | ATV212: Can the program file be saved to the HMI keypad, VW3A1101? No. With the ATV212, the programming cannot be saved to any of the keypads available. Programming can be saved by three methods:
- in the drive... |
| FA168139 | Does the ATS48 include a shorting contactor? No. To have the shorting contactor feature, a separate contactor needs to be wired to the ATS48.
CTA-ID : 2062873 |
| FA168131 | When do the ATS48 cooling fans run? ATS48D17Y and ATS48D22Y do not have fans. All other models do have fans.
The fans will operate when the heatsink temperature is greater than 50C.
The... |
| FA168116 | Can the ATS46 keypad be used in direct sunlight? No. The display cover is not UV protected. The display will not function properly if exposed to direct sunlight over time.
CTA-ID : 2062705 |
| FA168122 | Are the ATS48 keypads UV protected from direct sunlight? The remote terminal VW3G48101 is delivered as a kit comprising:
- the keypad,
- a mounting kit containing a cover, screws and an IP 54 seal on the... |
| FA168124 | Can the ATS48 run in a test mode when a motor is not connected? No. The unit must have output current or it will fault on PHF. For testing purposes, setting menu drC, parameter SSt = ON allows the use of a small... |
| FA168179 | Do the ATS22 products have an internal contactor? Yes. It is a shorting contactor that closes when the motor is up to full speed. The purpose is to give the current a path around the SCRs. This... |