| FA164397 | Can I use the ATV61/71 HMI keypad, part number VW3A1101, on a Altivar 31 drive? No. The ATV61 / 71 keypad can be used on the ATV312 drives, but not on the ATV31 drives. See remote keypad part number VW3A31101 for the ATV31 drives.... |
| FA109470 | How can part numbers be found for Econoflex drives? The econoflex drive has so many possible combinations of features that it is impractical to have part numbers. It is a product that is quoted, ordered... |
| FA109851 | What replaces the 8839TR01 ATV66 High Ambient Unloader since it is listed as obsolete? The kit includes three items: a thermistor (available only from SQD as part number 26116-78101), a 3.32kohm 1/4 watt 1% resistor (available from... |
| FA97661 | Can a Powerlogic Monitor or Power Meter be selected in Q2C Product Selectors? No. These options and related components must be priced in notepad per the SW-2A Pricing Guide. This document is available via the Intranet or by... |
| FA100079 | How are products ordered for a Habitat for Humanity (HFH) project? The Local HFH Affiliate should log onto the HFH secure extranet site, Partnernet, and download the Square D order form and instructions. The appropriate... |
| FA146135 | How do you get the LSU software for the UTA Tester? Download from this site:
http://www.schneider-electric.us/sites/us/en/support/product-support-resources/software-and-calculators/software/ltu-software-for-uta-tester.page
Alternatively,... |
| FA130457 | Where is support available for Xantrex inverters - Mobile Products ? Xantrex is in Vancouver, CN . General Tel: 604.422.8595 , or for Technical and customer support call toll free 800-670-0707(For Schneider Electric... |
| FA127196 | Has part number HU1003MC6 but Q2C states customer not authorized to purchase Use part number 80439-889-54 and force on Seneca.CTA-ID : 2049566 |
| FA127086 | Needs part number for Model 6 200 Amp fuse clip Part number will be 40555-127-50 and will need a quantity of 6 , Same clip is used fro Class H, J and R, if class R you will need a HRK-1020 quantity... |
| FA127054 | Do we include unit nameplates as standard in MCC units. If a Standard MCC is selected unit nameplates are not provided as standard but can be selected. If a Industrial MCC is selected nameplates are supplied... |