| FA167053 | What is the replacement cover for a QO2040MW200, series L8? The load center is very old and obsolete and the cover part numbers were either a QOC20MW225S(surface) or QOC20MW225F(Flush). They are both OBSOLETE... |
| FA167052 | What are the repair parts for a QO30M200RB, Series G1, Load Center? Only the parts listed below are considered field replacable.
Cover - 4054802204
Interior trim - 4054507701 (This Trim is Obsolete and No longer available... |
| FA167051 | What is the replacement module for TVS5EMA32A? Each phase has 2 - MA5IMA16 modules. |
| FA167022 | The UTS3 test set does not trip the LX type breaker on the trip solenoid test but the breaker still trips for overcurrent tests; is the breaker bad? The trip solenoid used on the LX and LE breaker has a greater range of power requirements than the UTS3. Therefore, it is possible that the UTS3... |
| FA92450 | Should the Omegapak 8804 PT capactiors be replaced if the unit has been sitting for a while? Whether the capacitors need to be replaced may depend on how long the unit has been sitting.Also, while they may not need to be replaced, it may be... |
| FA166729 | What is the catalog number for clamps used with panelboard enclosure, MH62WPSSULNQ This box is purchased from an outside vendor, EMF Electrical Enclosures and their toll free number is 800-338-6727
CTA-ID : 2058555 |
| FA166702 | What is the non interplant part number that can be used to order a replacement 80034-187-02 (interplant part number) filler plate? The part number that can be ordered for a customer is HLW1BL.
CTA-ID : 2058664 |
| FA166695 | What are the kit contents of the NQCUM2 main lug kit? The NQCUM2 consist of the following parts:
(1) Neutral mechanical lug
(3) Main mechanical lugs
(3) 1/4-20 x 7/8-inch tapping screws
(1) 1/4-20... |
| FA166684 | What parts are included in the NF400FTL 400A Feed-Through Lug Kit? The parts included in the NF400FTL kit include:
(1) Neutral lug
(3) Feed-through lugs
(4) 10-32 x 5/16 in tapping screws
(2) 1/4-20 x 7/8 in tapping... |
| FA166683 | What is included in the NQSFL4 400A Sub-Feed Lug Kit? The parts included in the NQSFL4 Sub-Feed Lug kit include:
(1) Neutral lug
(3) Line lugs
(2) 1/4-20 x 11/16 in tapping screws
(6) 1/4-20 x 7/8 in... |