Narrow By
  1. Your SelectionAll

Inoperative - FAQs

FAQ Search
Most Recently Published FAQs

Results 1 - 10 of 100

FAQ ID Description
FA170982Where do we send drives and soft starters back to get them repaired?
Contact Schneider Electric Industrial Repair Services 235 Burgess Rd.     Greensboro    NC 27409 Phone number is (336) 668-4848   FAX: 336.668.4878 ...
FA169579How can I get rid of a CF12 fault when using PC Soft on an ATV212 drive?
body { margin: 0 0 0 0; padding:0 0 0 0 } td,div { font-family:;font-size:11pt;vertical-align:top } /* Copyright IBM Corp. 2011 All Rights Reserved....
FA168592Micrologic P or H trip unit says `com module not available` on the screen. What does this mean?
The trip unit is not communicating with the breaker comms module (BCM).  Either the comms module is bad, does not exist, or is not powered up with...
FA168176On the ATV212 drive, what causes an nSt fault?
Most parameters cannot be changed while the motor is running.  If such a parameter is changed when the motor is running, the drive will freewheel...
FA168170On an ATV212, what does a flashing E-17 code mean?
This code indicates that a keypad button has been depressed for more than 20 seconds.  Release the depressed button to clear the fault.  Attempt to...
FA168137ATV212: Added the remote keypad, VW3A1101. When powered up, the display stays at CONNECTION IN PROGRESS.
Verify the following parameters: F800=1 F801=1 Also, the keypad Flash must be V1.1IE29 or higher.  Check the label on the backside. CTA-ID : 2062274
FA167980ATV61 is tripping on Ground short circuit (SCF3) fault.
Measure across L1,L2,L3 and DC Bus across PA/+ and PC/- and PO to PC. Do a static check on the front end of the drive with diode checker on a Multimeter. PO...
FA164112What does a flashing E on the ATV212 display mean?
The drive is in a faulted status, initiated by one of the following:1) CMOd is set to 0 or 2, the drive is in remote mode and the keypad STOP button...
FA164705What is an O.CF fault on an ATV31?
O.CF is a phase-to-phase motor short circuit fault.  Check motor windings and motor leads for a possible shorting path.Other possible related fault...
FA167393What causes an StF fault on an ATS22 soft starter?
The StF fault means the starter has exceeded the maximum start time setting tLS in the SEt menu.   tLS needs to be set higher then the ACC time.  ...

Results 1 - 10 of 100