Narrow By
  1. Your SelectionAll

Cross Reference - FAQs

FAQ Search
Most Recently Published FAQs

Results 91 - 100 of 100

FAQ ID Description
FA130388Want to add a CE3040H to an existing CDP panel?
The CE3040H breaker is obsolete. The Replacement breaker is a Square D HLL36040 breaker with a HDCMH mounting kit. The HLL breaker is rated 50KAIC...
FA130406Want to add a CE3040E to an existing CDP panel?
The CE3040E breaker is obsolete. The Replacement breaker is a Square D HGL36040 breaker with a HDCMH mounting kit. This breaker is rated 18KAIC at...
FA130392Want to add a CE3060B to an existing CDP panel?
The CE3060B breaker is obsolete. The Replacement breaker is a Square D HDL36060 breaker with a HDCMH mounting kit. This breaker is rated 14KAIC at...
FA130390Want to add a CE3030B to an existing CDP panel?
The CE3030B breaker is obsolete. The Replacement breaker is a Square D HDL36030 breaker with a HDCMH mounting kit. This breaker is rated 14KAIC at...
FA130387Want to add a CE3090H to an existing CDP panel?
The CE3090H breaker is obsolete. The Replacement breaker is a Square D HLL36090 breaker with a HDCMH mounting kit. The HLL breaker is rated 50KAIC...
FA130404Want to add a CE3070H to an existing CDP panel?
The CE3070H breaker is obsolete. The Replacement breaker is a Square D HLL36070 breaker with a HDCMH mounting kit. The HLL breaker is rated 50KAIC...
FA130397Is a 120 volt replacement control coil available for LC1D2510?
No, the part #`s LX1D4G6 for 60 hertz or LX1D4G7 for 50/60 hertz are obsolete with no replacement. Suggest replacing the device with contactor...
FA130354Want to add a CE3050E to an existing CDP panel?
The CE3050E breaker is obsolete. The Replacement breaker is a Square D HGL36050 breaker with a HDCMH mounting kit. The breakers are rated at 18 KAIC.The...
FA130352Want to add a CE3050B to an existing CDP panel?
The CE3050B breaker is obsolete. The Replacement breaker is a Square D HDL36050 breaker with a HDCMH mounting kit. The breakers are rated at 14 KAIC.The...
FA130351Want to add a CE3150B to an existing CDP panel?
The CE3150B breaker is obsolete. The Replacement breaker is a Square D HDL36150 breaker with a HDCMH mounting kit. This breaker is rated 14KAIC at...

Results 91 - 100 of 100