| FA144487 | Do we offer a cross for a 2936-S1-C32B, 440 -480V coil? No, the 2936S1C32B coils are obsolete with no replacement. They will need to replace the complete contactor / starter. CTA-ID : 2059522 |
| FA144513 | What is the replacement for the 29340 handle mechanism kit? The catalog number has been changed to globally align the numbering system.
The 29338 is the standard black handle replaced with the part numberĀ ... |
| FA143606 | What can be used to replace a XACS105 contact block? Order as a XACS101 and ZB2BE102.
CTA-ID : 2059606 |
| FA142737 | Is the ZB4BPA replacement for the ZB4BP the same 22mm clear booted flush pushbutton? Yes. The following crosses are to align globally our current catalog or part identification numbering sytstem:
ZB4BP1 ZB4BPA1 NON-ILLUM CLEAR BOOT... |
| FA130151 | To add a CE3175H to an existing CDP panel? The CE3175H breaker is obsolete. The Replacement breaker is a Square D JLL36175 breaker with a JDCMH mounting kit. This breaker is rated 50KAIC at... |
| FA130111 | Want to add a CE3030E to an existing CDP panel? The CE3030E breaker is obsolete. The Replacement breaker is a Square D HGL36030 breaker with a HDCMH mounting kit. This breaker is rated 18KAIC at... |
| FA99815 | What is the replacement for a HOM2PL padlock attachment. Use HOM2PALA for 15 - 70 ampere Homeline circuit breakers. Use HOM2PAHA for 80 - 125 ampere Homeline circuit breakers. CTA-ID : 2003143 |
| FA100077 | What can be used in the place of the 8440 PS power supplies? We have no power supplies this small at this time. The ABL7`s can be used as a replacement. The ABL7RP1205 has a 5A 12 volt DC output capacity.... |
| FA131327 | Is there an replacement 120V coil, part number 31021-400-60 for the 8501G magnetic relays? No, the 31021-400-60 is obsolete with no replacement. CTA-ID : 2055420 |
| FA131253 | The XMLA070D2S11 is the recommended replacement for the XMLA070D1S11. What is the difference between the nomenclature D1 and D2?
The D1 has no display the D2 has a display. CTA-ID : 2055419 |