| FA107757 | What unit is the current replacement for the obsolete VSD07 ? Check the voltage and amperage ratings.For most of the 120, 208 & 230 VAC single or three phase input ratings use the ATV11 with the same Amp rating.For... |
| FA99863 | Does Square D have a cross reference to a Midwest catalog number U038C010? The Square D equivalent is PAK72C. CTA-ID : 2003868 |
| FA110928 | What is the cross reference for the XCKJ*910 interlock switch? Visit the Online competitive cross reference tool via the above attachments tab. CTA-ID : 2019271 |
| FA100451 | What is the cross reference for the XCKJ*970 interlock switch? Visit the Online competitive cross reference tool via the above attachments tab. CTA-ID : 2005378 |
| FA87252 | What is the replacement for a 9001LMA1? This is a light module for an obsolete 22mm operator. The 9001 Type L devices are all obsolete with no replacement parts. The entire device must... |
| FA87983 | What is the cross reference for XCKP791 ? Visit the Online competitive cross reference tool via the above attachments tab. CTA-ID : 1323 |
| FA101134 | What is the replacement for an XSFA155549 ? Use cross reference tool below. CTA-ID : 2005829 |
| FA146133 | Can I still purchase a 999320? The 999 series is a ML1 and was replaced by an FAL and SK4515. The SK4515 kit is now obsolete and no longer available.
CTA-ID : 2060107 |
| FA145350 | What replaces the AM1DP200? 9080MH379.
CTA-ID : 2060102 |
| FA144668 | What is the replacement for a 9001TB contact block?
This was 2 NO and 2 NC contacts. The 9001TAD1 adapter that allowed using the 9001KA1 contacts is obsolete. Entire operator will need to be crossed... |