Narrow By
  1. Your SelectionAll

Cross Reference - FAQs

FAQ Search
Most Recently Published FAQs

Results 41 - 50 of 100

FAQ ID Description
FA88377What is the cross reference for a XCKJ5910547?
Visit the Online competitive cross reference tool via the above attachments tab. CTA-ID : 2179
FA88093What is the cross reference for a XSPH08362?
Visit the Online competitive cross reference tool via the above attachments tab. CTA-ID : 2266
FA98161What is the cross reference for a 9007B53B2 limit switch?
Visit the Online competitive cross reference tool via the above attachments tab. CTA-ID : 2000789
FA87361Can the LR2D bimetallic overload relays be used as a replacement for the LR1D bimetallic overloads that were direct mounted to the LC1D pre-TeSys contactor?
Yes, however if the unit is enclosed the external reset mechanism will not align with the reset on the replacement overload relay.Please use the link...
FA111131What has replaced the obsolete XUGF04031 sensor?
Visit the Online competitive cross reference tool via the above attachments tab. CTA-ID : 2020369
FA103608What is the replacement for a Q12150 mounted in a QO load center?
It may be possible to replace the Q12150 with a QO2150. The QO2150 can be applied in a Square D QO SINGLE PHASE load center, Series G1 (see Note #1),...
FA111194What replaces the XM2JM0122 pressure switch?
Visit the Online competitive cross reference tool via the above attachments tab. CTA-ID : 2020396
FA109897What is the replacement for a 9038CG1 float switch?
See the competitive cross reference tool below.. CTA-ID : 2018214
FA99509What is cross reference for a 9037HR4S1?
Visit the Online competitive cross reference tool via the above attachments tab. CTA-ID : 560
FA107904What is the cross reference for the 9007B54J limit switch?
Visit the Online competitive cross reference tool via the above attachments tab. CTA-ID : 2001732

Results 41 - 50 of 100