| FA98678 | Do EDB breakers have the CE mark? Yes. See documentation under International Information on Codes and Standards homepage under LEGAL on Intranet. CTA-ID : 2000719 |
| FA98633 | Do SFI breakers have the CE mark? Yes. See documentation under International Information on Codes and Standards homepage under LEGAL on Intranet. CTA-ID : 2000726 |
| FA98634 | Do SKC breakers have the CE mark? Yes. See documentation under International Information on Codes and Standards homepage under LEGAL on Intranet. CTA-ID : 2000727 |
| FA98635 | Do SLA breakers have the CE mark? Yes. See documentation under International Information on Codes and Standards homepage under LEGAL on Intranet. CTA-ID : 2000728 |
| FA98630 | Do MA and MH breakers have the CE mark? Yes. See documentation under International Information on Codes and Standards homepage under LEGAL on Intranet. CTA-ID : 2000721 |
| FA98631 | Do LC and LI breakers have the CE mark? Yes. See documentation under International Information on Codes and Standards homepage under LEGAL on Intranet. CTA-ID : 2000722 |
| FA108253 | What will the coils on a 8501 type K relay operate at? The will operate at AC: +10, -15% of Nominal Voltage at 25 deg C (77 deg F)They will operate at DC: +10, -25% of Nominal Voltage at 25 deg C (77 deg... |
| FA98679 | Do SFA and SFH breakers have the CE mark? Yes. See documentation under International Information on Codes and Standards homepage under LEGAL on Intranet. CTA-ID : 2000723 |
| FA98629 | Do PA and PH breakers have the CE mark? Yes. See documentation under International Information on Codes and Standards homepage under LEGAL on Intranet. CTA-ID : 2000720 |
| FA146359 | Are the earth leakage modules ELM150HD and ELM250JD rated for use at 50 hertz. ELM modules are dual 50/60hz rated . CTA-ID : 2060246 |