| FA163572 | Is the remote racking device for Masterpact NW breakers NWMPRRT UL Listed and/or CSA approved? It is neither UL Listed nor CSA approved.
CTA-ID : 2061093 |
| FA162163 | Is an NFNL36030 CE marked? Yes. This breaker is now obsolete.
CTA-ID : 2060931 |
| FA152243 | Do the NQ, NF and I-Line panels meet IEC 60439-1 standards ? Yes
CTA-ID : 2060606 |
| FA126995 | Is the 82255 UL listed? Yes, this device is UL listed and is labeled cULus, File E-2875. CTA-ID : 2048599 |
| FA126682 | Is the 82445 UL listed? Yes, this device is UL listed and is labeled cULus, File E-2875. CTA-ID : 2048612 |
| FA126998 | Is the H82345 UL listed? Yes, this device is UL listed and is labeled cULus, File E-2875. CTA-ID : 2048611 |
| FA126683 | Is the H82445 UL listed? Yes, this device is UL listed and is labeled cULus, File E-2875. CTA-ID : 2048614 |
| FA126999 | Is the 82445R UL listed? Yes, this device is UL listed and is labeled cULus, File E-2875. CTA-ID : 2048613 |
| FA126681 | Is the 82345DS UL listed? Yes, this device is UL listed and is labeled cULus, File E-2875. CTA-ID : 2048610 |
| FA126997 | Is the 82455R UL listed? Yes, this device is UL listed and is labeled cULus, File E-2875. CTA-ID : 2048607 |