Narrow By
  1. Your SelectionAll

Assembly/Installation - FAQs

FAQ Search
Most Recently Published FAQs

Results 71 - 80 of 100

FAQ ID Description
FA129394The elbow has been connected to the vault box 180 degs in the opposite direction. We need to re-do the connection between the elbow and the box. Need service to fix before the end of next week
Elbow was rotated 180 degrees.CTA-ID : 2052775
FA129365What positions can the 9013FSG2 be mounted in?
Any position. CTA-ID : 2052409
FA129232What is the maximum AC mains wire distance allowable to connect an SDSB1175C surge suppressor to a panelboard or load center?
The wire length should be very short, about 18 inches from the panel bussing, maximum. Longer lengths drastically reduce the effectiveness of the...
FA129125What is the part number for the neutral bus kit for an 400A QMB panelboard?
It is the QMB4SN.CTA-ID : 2051742
FA129108What standard applies to operating handle heights on switchgear?
NEC 490.41The maximum height we should install any hand operated device is 6`6``(78 in.) unless it is a switch handle requiring more than 50 lbs....
FA129072LC1D12G7: How do you panel mount this?
There are screw holes in the upper right and lower left corners of the contactorCTA-ID : 2051529
FA129129A customer is wanting to prepare a pad for some outdoor switchgear on order.
How much distance should be allowed around the switchgear?
5 feet is recommended on all sides.CTA-ID : 2050972
FA128929Can a vertically mounted 8702SE or SF NEMA contactor be field converted to horizontal mounting?
Yes, use a 9999SM12 horizontal interlock. The customer will have to supply their own power wiring.CTA-ID : 2051337
FA128927What are the torque requirements for QO wire binding screws and clamp plates?
Scroll down for complete information.QO/QOB 10A - 30A, 1,2 and 3-pole, all interruption ratings: 36 lb.-in.QO/QOB 35 - 70A, 2 and 40 - 60A 3-pole,...
FA128896Does an energy efficient transformer have to be de-energized to install a weathershield?
ABSOLUTELY!! Whenever work is being done on an electrical device, the power to the device needs to be turned off. In this case, the front and rear...

Results 71 - 80 of 100