Narrow By
  1. Your SelectionAll

Assembly/Installation - FAQs

FAQ Search
Most Recently Published FAQs

Results 31 - 40 of 100

FAQ ID Description
FA98190What is the torque for the MLO lug set-screw and lug bolt 1000A HCW2353-12?
Lug set screw - 340 in/lbs.1/2`` KEPS nut w/ al terminals:  #2 - 600MCM CU-AL (1/2`` socket) - 38 ft lbs.1/2`` KEPS nut w/ cu terminals:  #2 - 600MCM...
FA98559Does the MCT-CT (remote control unit for a MCT-12B digital clock/timer) come with a back box and if not what is used?
The back box is not supplied by Square D.  Simply utilize a 2 gang back box  that is at least 3.25`` deep.  This is shown on page 53 of the Hospital...
FA111067How are melting alloy thermal units mounted into 9065 overload blocks?
To properly mount the thermal units, installers should:1 - Remove all power from the controller;2 - Hold the thermal unit so the ratchet / geared...
FA102177Does an MCT-12B or MCT-14B clock/timer require a back box? If so, what is the appropriate catalog number?
When the MCT-12B is installed in the Surgical Facility Panel, no additional components are required.  When the MCT-12B is to be mounted in a wall,...
FA103115What would cause an XCKT Limit Switch to allows fluid into the switch?
Mounting the limit switch under water (or other fluid) and attempting to operate it there will cause leaks.   Exposure to wide temperature swings...
FA144773Why is there a gap in the bussing in a EZM1800FS, between the MHP26000 switch and thru bus?
The gap is where 300VAC Class T fuses are to be installed. CTA-ID : 2060026
FA143594What is the torque requirement for lugs for the Powerpact L frame breaker?
The torque requirement for the following lugs is 50 N-m or 442 lb.-in. AL400L61K3, AL600LS52K3, CU600LS52K3, AL600LF52K3, CU600LF52K3 The torque...
FA107614How can you mount the main breaker kit to an NF main lug interior and have it all fit in the same enclosure?
This can not be done in the same enclosure. The enclosure will not stay the same . A larger box and trim must be ordered. The size can be determined...
FA108877What is the part number for the interior mounting hardware bag assembly for a 400A or 600A NF panel?
80114-251-51 This bag assembly contains the hardware required to mount the interior in the enclosure, circuit numbers and information manual. ...
FA99980What are the rail and deadfront extensions required to mount an NQOD442L225 or NQOD442L225CU in an MH50 or MH50WP?
The following parts will be required per panel and can only be mounted at the mains end:(2) 80110-288-05 15`` rail extensions(1) 80110-291-04...

Results 31 - 40 of 100