Narrow By
  1. Your SelectionAll

Assembly/Installation - FAQs

FAQ Search
Most Recently Published FAQs

Results 11 - 20 of 100

FAQ ID Description
FA165171Can an overload relay be field installed in a LE1D123A62OG70 enclosed starter?
Yes there will be enough space in the enclosure to install the proper overload relay in the field. CTA-ID : 2061130
FA164428Will the Powerpact H breaker fit into an old NH1B panelboard?
No.  We do not have any mounting assemblies to allow the H frame breaker to install into that panel. CTA-ID : 2054364
FA163895What is the S suffix on the ATV212HD22N4S drive?
body { margin: 0 0 0 0; padding:0 0 0 0 } td,div { font-family:;font-size:11pt;vertical-align:top } /* Copyright IBM Corp. 2011 All Rights Reserved....
FA163560How do you mount an NQSFL1 sub feed lug kit?
Remove the main lugs and replace with the lugs from the kit. CTA-ID : 2055475
FA162017Can wall duct be surface mounted on the floor?
Wall duct may be used as surface mounted to the floor. CTA-ID : 2060924
FA162016Can trench duct be surface mounted to the floor?
Trench duct can not be surface mounted to the floor. Trench duct is designed to be encased in cement. Wall Duct may be used as surface mounted to...
FA152196How do you field convert the 8903 Type L or Type LX power contacts from normally open to normally closed?
See contact conversion steps listed in the instruction bulletin 30072-013-31 for 8903L and bulletin 30072-013-32 for the 8903LX. CTA-ID : 2060482
FA93315Where is the KLC output filter mounted relative to the drive and the motor?
KLC filters are designed to be located immediately adjacent to the output terminals of the drive and to be wired directly to the drive output. The...
FA113543Does the ATV31 have a sleep mode?
Yes.Go to the SET menu and scroll down to parameter tLS (Low Speed Operating Time). After operation at LSP for a defined period, a motor stop is requested...
FA119333What I-O points are available on the standard Altivar 61 and 71 drives?
Below are the Inputs and Outputs that are on board without adding options:Analog input #1: +/- 10Vdc bipolar input, 1 bits + 1 signresolution, 2ms...

Results 11 - 20 of 100