| FA114924 | Can multiple motors be connected to one solid state soft starter? Yes. Size the soft starter for the total full load amps of all motors to be connected.Provide separate overload protection for each motor.Motor connections... |
| FA103864 | Are Square D Heavy Duty Switches UL Listed for use on photovoltaic (solar) applications? Please refer to the Data Bulletin 3110DB0401R09/09, Dated 11/2009, link provided below. The wiring diagrams shown on Page 1, Figures 1B, 1D or 1F... |
| FA118572 | What is the terminal lug data for the QO200TR?
The ``line side`` terminal lug wire size is #14 to #4 AWG AL/CU and the ``load side`` terminal lug wire size #14 to #6 AWG AL/CU. The grounding... |
| FA122748 | Can a PAK41PG be mounted directly to ACQ (Alkaline Copper Quaternary) Pressure-Treated wood? The chemical compounds used in ACQ preserved wood products may have an adverse effect on the metal enclosure and the fasteners used to secure the... |
| FA122749 | Can a PAK61PG be mounted directly to ACQ (Alkaline Copper Quaternary) Pressure-Treated wood? The chemical compounds used in ACQ preserved wood products may have an adverse effect on the metal enclosure and the fasteners used to secure the... |
| FA122750 | Can a PAK75PG be mounted directly to ACQ (Alkaline Copper Quaternary) Pressure-Treated wood? The chemical compounds used in ACQ preserved wood products may have an adverse effect on the metal enclosure and the fasteners used to secure the... |
| FA123223 | Can a PAK61CTG be mounted directly to ACQ (Alkaline Copper Quaternary) Pressure-Treated wood? The chemical compounds used in ACQ preserved wood products may have an adverse effect on the metal enclosure and the fasteners used to secure the... |
| FA122809 | Can a PAK41CTG be mounted directly to ACQ (Alkaline Copper Quaternary) Pressure-Treated wood? The chemical compounds used in ACQ preserved wood products may have an adverse effect on the metal enclosure and the fasteners used to secure the... |
| FA122808 | Can a PAK11CTG be mounted directly to ACQ (Alkaline Copper Quaternary) Pressure-Treated wood? The chemical compounds used in ACQ preserved wood products may have an adverse effect on the metal enclosure and the fasteners used to secure the... |
| FA122807 | Can a PAK10CTG be mounted directly to ACQ (Alkaline Copper Quaternary) Pressure-Treated wood? The chemical compounds used in ACQ preserved wood products may have an adverse effect on the metal enclosure and the fasteners used to secure the... |