| FA163719 | Are Series Rating available for QO Main Lug Only, 1 Phase load centers when using std QO 10,000 AIR branches ? Series Ratings for current design Series S01 and S02 (Convertible Mains), 125 - 225 ampere, Main Lug Only, 1 Phase QO load centers include:
100,000... |
| FA163611 | Can you do a multipoint addressing with the ATV312 drives?
It is not possible to do multipoint addressing with the ATV312 drives. The menu for the configuration can be displayed on the remote HMI but... |
| FA163564 | Can a NQ, 84 circuit 400A panelboard be provided with a sub feed breaker? No, we do not offer a box larger enough to accomadate a sub feed breaker kit in a 84 circuit NQ Panelboard.
CTA-ID : 2055122 |
| FA130908 | Is the Zelio Smart Relay software - SR2SFT01 compatible with Windows 7? The software is compatible with Windows 98, NT, 2000, XP, ME and Windows 7. CTA-ID : 2055098 |
| FA162393 | How many S29450 can be mounted in a PGL breaker? It has place for (3) auxillary contact and (1) alarm switch and (1) overcurrent switch.
CTA-ID : 2061081 |
| FA162181 | What is the replacement pullout only for a FTL2100? 4050704950, The replacement pullout is OBSOLETE and NO LONGER AVAILABLE.
CTA-ID : 2060765 |
| FA116066 | Is there a restriction for a breaker mounted opposite 125 amp ED, EG, or EJ breakers? Yes, the ampacity of the breaker mounted opposite cannot exceed 20 amps. CTA-ID : 2027586 |
| FA115737 | How many EDB34125`s can be installed in an NF panel?
If enclosure is a NEMA 3R , just one can be mounted in 400/600A panels. If box is a NEMA 1 ,more than one can fit in a 400A/600A panel . If 125A... |
| FA162002 | REJECTED: THIS INFORMATION IS STILL NEEDEDAre KA/KAL 2 pole breakers rated for use at 250 Vdc? REVISION TO RESOLUTION 2023187: KA/KAL BREAKERS ARE NOW OBSOLETE.
Yes, 2 pole breakers are good for 10k AIR at 250v DC. Note the 3p breakers can... |
| FA113738 | Can you rotate the NF panel for opposite feed? Yes, turn the panel interior 180 degrees. If the panel has a vertically mounted main breaker turn it 180 degrees also. Turn the branch breaker portion... |