| FA93817 | What is the part # for a stud for an I-Line HC style Nema 1 box? The 1/2``-13 threaded stud part # is 80025-040-01, and the keeper nut is 23304-02801. CTA-ID : 9828 |
| FA164352 | ATV21 or ATV212 BACnet configuration assistance.
BACKGROUND:
BACnet is an open Communication Protocol that was developed by ASHRAE (American Society of Heating, Refrigerating, and Air-Conditioning... |
| FA164562 | If the correct Homeline load center has the HOMCRBGK1 generator interlock kit installed and the utility power is OFF with the generator power ON, Will the Load Center main breaker automatically come ON if Utility Power is restored while the generator is running? NO, the HOMCRBGK1 is a MANUALLY operated generator interlock kit, which restricts the load center main breaker from being ON while the generator breaker... |
| FA164381 | Can the ATV66 standard drive accept an encoder feedback? No, but you can use a converter to convert the encoder signal to a 0-10V or 4-20 (0-20) ma and use it to control the speed.
CTA-ID : 2061425 |
| FA164390 | How many Preset Speeds does the Altivar 61 support? The Altivar 71 product line supports up to 16 preset speeds including the Low Speed setting.
Preset speeds can be selected under the Menu 1.7 Application... |
| FA164386 | What is the maximum number of AFI breakers in an NQ panelboards? Maximum is (28) per the product selector because of pigtails not being able to reach the neutral. However, pigtails can be spliced in the factory... |
| FA164392 | How many Preset Speeds does the Altivar 71 support? The Altivar 71 product line supports up to 16 preset speeds including the Low Speed setting.
Preset speeds can be selected under the Menu 1.7 Application... |
| FA164427 | Can you replace an MAP36800 main breaker with an MJP36800 in an I Line panel? No . There are several dimensional differences
CTA-ID : 2057957 |
| FA164404 | Is there a limit to how many GFI breakers can be put into an NQ panel ? No, although product selector does have a limit of 28 based on pigtail length, pigtails can be spliced in the factory and the field.
CTA-ID : 2057946... |
| FA100284 | Can an NQOD with an 8903 PB lighting contactor main be rated 42k AIC? The contact must be protected by a circuit breaker rated 42k AIC or higher. The contactor cannot meet this AIC rating as a stand alone device. CTA-ID... |