| FA127765 | What type main breaker is used in the NQ8430B1C? QOU3100 main breaker. CTA-ID : 2050469 |
| FA167048 | Can the GC200 Ground fault relay be used with two CT`s (sensors) from two different sources? Basically monitoring two separate circuits? No. This has not been validated. |
| FA167046 | Can the EasyPact breaker be reverse fed? Yes, the EasyPact circuit breaker can be supplied from either the top or the bottom (reverse feeding) without any reduction in performance.
Note that... |
| FA167045 | Is there a maximum number of receptacles that can be fed from one HOM-GFI breaker? No, but the circuit length must be under 250 ft. one way. |
| FA166747 | Will a QO3125SL subfeed lug kit fit into an NQ panelboard interior? Yes it will if application does not exede 125 Amps.
CTA-ID : 2058818 |
| FA166705 | What are the blanks extensions HLW4EBL and HLN4EBL used for? HLW4EBL is for use with for H and J frame breakers with Micrologic trip units 5 or 6 mounting on the wide side of an I-line panelboard.
HLN4EBL... |
| FA166731 | 9037EG9: does this include the float & rod? No, it is just the float switch. The kits must be ordered separately.
CTA-ID : 2061853 |
| FA166707 | How can you program the ATV212 Sflex to be reverse acting when using a 0-10V signal on VIB? They want 0V signal to be 60hz and 10V signal to be 0hz. Programmed the drive as follows:
F210 - 0 %
F211 - 60.0 Hz
F212 - 100 %
F213 - 0.0 Hz
and wire your 0-10vdc signal to VIB and CC
Fnod needs to be... |
| FA166690 | Can the ATV61 or ATV71 be installed in an ATEX environment? The ATV61 and ATV71 can be used in the functional safety loop for an ATEX application; however, they cannot be installed in the ATEX environment.... |
| FA166359 | What is the ATV61 drives part number for a variable torque application like a fan or pump?
The ATV61 drives are rated to be used on light loads like Fan and pumps. They range from 1HP up to 900 HP @ 480VAC 3phase, 1HP to 125HP @ 230VAC... |