| FA152228 | Is a line isolation contactor or shunt trip circuit breaker needed with Schneider Electric ATS48 soft starters? Since the solid-state switches may be incapable of completely blocking the motor power should a fault occur, auxiliary isolation on the line side... |
| FA167592 | How can the ATS22 be set up for automatic restart? There is not a specific parameter to program for an auto restart feature. However, this function can be accomplished per the following:
Set LI3 =... |
| FA163715 | What is a QO124L125PG? This is a new style of QO Load Center, referred to as ``PoN`` (Plug on Neutral), that has a specially designed branch neutral assembly that will accept... |
| FA167448 | Do ground fault trip units and relays still work on a 277/480V 3 wire 3 phase grounded system without a neutral? Yes. On a 3 phase 3 wire 277/480V grounded system with no neutral the trip unit ground fault function still works. The trip unit still uses the... |
| FA167414 | Do you have to derate the ATS48 Soft Starters if you mount them at high elevations? Yes,
Maximum operating altitude
3300 feet without derating. Above this, derate the nominal current by 2.2% for each additional 330 feet to the... |
| FA167385 | Can the ATS01 starter be installed after a contactor that only breaks 2 of the 3 phases to the motor? No. All 3 phases must be made to the starter to soft start the motor. The contactor also needs an overload relay because the ATS01 does not provide... |
| FA127765 | What type main breaker is used in the NQ8430B1C? QOU3100 main breaker. CTA-ID : 2050469 |
| FA167048 | Can the GC200 Ground fault relay be used with two CT`s (sensors) from two different sources? Basically monitoring two separate circuits? No. This has not been validated. |
| FA167046 | Can the EasyPact breaker be reverse fed? Yes, the EasyPact circuit breaker can be supplied from either the top or the bottom (reverse feeding) without any reduction in performance.
Note that... |
| FA167045 | Is there a maximum number of receptacles that can be fed from one HOM-GFI breaker? No, but the circuit length must be under 250 ft. one way. |