Narrow By
  1. Your SelectionAll

Application - FAQs

FAQ Search
Most Recently Published FAQs

Results 1 - 10 of 100

FAQ ID Description
FA170916SFlex ATV212 drive with a VW3A1101 ATV61 keypad shows connecting in progress on the HMI.
You need to make sure RJ45 modbus baud rate and Parity are both set to 1. F800= 1 F801=1
FA169579How can I get rid of a CF12 fault when using PC Soft on an ATV212 drive?
body { margin: 0 0 0 0; padding:0 0 0 0 } td,div { font-family:;font-size:11pt;vertical-align:top } /* Copyright IBM Corp. 2011 All Rights Reserved....
FA170423ATV61 - EFlex - noise causing 4-20mA signal latching one 20mA.
FA169717How can you copy a old ATV31 program into a new ATV312 drive?
This can be done if you set up your new ATV312 drive  ArE parameter needs to be set to 31E  or 31A. 31A has the knob on the face of the old ATV31...
FA106827Can an AC drive be used on a two speed motor?
Yes.The motor should be connected to the drive with the high speed windings. It is not necessary to use the low speed windings when connected to an...
FA120291Is tenant breaker QDP32200TM a direct replacement for the now obsolete QE3200VH as once used in EZMR, EZML and in EZMT 200A, 3-Phase Branch Units?
No.  EZMR, EZML and  EZMT 3-Phase, 200A  max. branch units were reconfigured and up-graded to now accept 225A  max. new style QDP32200TM family of...
FA168338Can a Powerpact M frame 3 pole breaker be used in a single phase application?
Yes, the breaker is labeled for single-phase use. CTA-ID : 2062901
FA165142What are the part numbers for early closing and late opening contacts for a 9001K, 9001SK, 9001KX, or 9001T operators?
9001KA5 is a normally closed late opening contact and a 9001KA6 is a normally open early closing contact.  These can be used together to provide overlapping...
FA168093How to set up Case 2 example on the ATV32 drive using devicenet assemblies 20/70 and 21/71?
See case #2 example on the following attachment.
FA164353How do you configure the ATV61 for BACnet communications?
ATV61 implementation of BACnet:     Hardware:           New Part # VW3A3319 after 2011 Old Part # VW3A3315 before 2011 Compatible with the ATV61...

Results 1 - 10 of 100