| FA171154 | ATS22: Is it ok to install a Square D surge suppressor SDSA3650 ahead of the Softstarter? |
| FA171086 | End of damper control for a Sflex ATV21 with bypass option.
End customers auto start will need to start up Damper Solenoid. Once the Damper is open you will need a damper relay to close (R) to indicate damper... |
| FA170916 | SFlex ATV212 drive with a VW3A1101 ATV61 keypad shows connecting in progress on the HMI. You need to make sure RJ45 modbus baud rate and Parity are both set to 1.
F800= 1
F801=1 |
| FA169579 | How can I get rid of a CF12 fault when using PC Soft on an ATV212 drive?
body { margin: 0 0 0 0; padding:0 0 0 0 }
td,div { font-family:;font-size:11pt;vertical-align:top }
/* Copyright IBM Corp. 2011 All Rights Reserved.... |
| FA170423 | ATV61 - EFlex - noise causing 4-20mA signal latching one 20mA. |
| FA169717 | How can you copy a old ATV31 program into a new ATV312 drive? This can be done if you set up your new ATV312 drive ArE parameter needs to be set to 31E or 31A.
31A has the knob on the face of the old ATV31... |
| FA106827 | Can an AC drive be used on a two speed motor? Yes.The motor should be connected to the drive with the high speed windings. It is not necessary to use the low speed windings when connected to an... |
| FA120291 | Is tenant breaker QDP32200TM a direct replacement for the now obsolete QE3200VH as once used in EZMR, EZML and in EZMT 200A, 3-Phase Branch Units? No. EZMR, EZML and EZMT 3-Phase, 200A max. branch units were reconfigured and up-graded to now accept 225A max. new style QDP32200TM family of... |
| FA168338 | Can a Powerpact M frame 3 pole breaker be used in a single phase application? Yes, the breaker is labeled for single-phase use.
CTA-ID : 2062901 |
| FA165142 | What are the part numbers for early closing and late opening contacts for a 9001K, 9001SK, 9001KX, or 9001T operators? 9001KA5 is a normally closed late opening contact and a 9001KA6 is a normally open early closing contact. These can be used together to provide overlapping... |