| FA167602 | What is the ATS22 adjustable range for ILt, current limit? The range is 200% to 700% of parameter In, motor rated current. The maximum is limited to 350% of the ATS22 amp rating.
If the application requires... |
| FA167597 | How can you change the monitoring screen to show different parameters other then frequency reference on the ATV61 and ATV71 drives? Under Main Menu,
Go into Menu 6 Monitoring Configuration.
6.2 Monitor Screen Type adjusts the number of parameters that can be displayed and the... |
| FA167444 | What are the Micrologic 5.0P ground fault alarm pick up and delay ranges? Pickup: 20 to 1200 amps, +/- 15%.
Delay: 1 to 10 seconds
CTA-ID : 2062500 |
| FA167414 | Do you have to derate the ATS48 Soft Starters if you mount them at high elevations? Yes,
Maximum operating altitude
3300 feet without derating. Above this, derate the nominal current by 2.2% for each additional 330 feet to the... |
| FA167056 | How can ATS22 be set for Freewheel Stop mode? Goto SEt menu and program dEC parameter to Free. |
| FA166888 | ATS22 soft start is tripping on SnbF and this code cannot be cleared. SnbF indicates that too many starts were attempted based on the settings for parameters Snb (number of starts) and SLG (starts period). The soft... |
| FA97528 | Can the In Phase Loss on the 8803 Omegapak be turned off? This can only be done on the CT style units and is changed using the Commissioning terminal (8803 PPO1 ) or PC software (no part number). Go to the... |
| FA166691 | How is the ATS22 set for 3 wire control? Wire the momentary normally closed STOP contact to LI1 and the momentary normally open START contact to LI2.
Program the ATS22. In the I-O menu,... |
| FA166743 | How can the ATV61 drive be prevented from going into reverse when the HMI dial is turned to the negative range? In Menu 1.6 COMMAND, set RV Inhibition to Yes. This also applies to the ATV71 drives.
Note that this does not prevent reverse operation when the... |
| FA166718 | How can frequencies be skipped in an ATV61 / ATV71 ? In menu 1.3 Settings, adjust the following parameters:
Skip Freq = desired frequency ( in the middle of the skip range )
Skip Freq Hysteresis = (+)... |