Narrow By
  1. Your SelectionAll

Adjustments - FAQs

FAQ Search
Most Recently Published FAQs

Results 1 - 10 of 100

FAQ ID Description
FA171156 How can I change the motor direction if the motor is rotating right in drive mode but not in bypass mode?
FA171155What is the step by step procedure to connect SoMove Lite to ATV61/71 drive via EtherNet/IP card VW3A3316?
FA171086End of damper control for a Sflex ATV21 with bypass option.
End customers auto start will need to start up Damper Solenoid.   Once the Damper is open you will need a damper relay to close (R) to indicate damper...
FA170916SFlex ATV212 drive with a VW3A1101 ATV61 keypad shows connecting in progress on the HMI.
You need to make sure RJ45 modbus baud rate and Parity are both set to 1. F800= 1 F801=1
FA170909How do you change the temperature units from Celsius to Fahrenheit on the REG48 and REG96 temperature controllers?
Adjusting displayed content Converting the temperature displayed from Celsius to Fahrenheit To change the REG48 or REG96 temperature controller...
FA170677What type of tap or termination can be added to a Modbus RTU RS485 Network to prevent network communication fault?
FA170686 How can you convert a Trane unit Flex58 over to an ATV61 open type drive?
FA170423ATV61 - EFlex - noise causing 4-20mA signal latching one 20mA.
FA169717How can you copy a old ATV31 program into a new ATV312 drive?
This can be done if you set up your new ATV312 drive  ArE parameter needs to be set to 31E  or 31A. 31A has the knob on the face of the old ATV31...
FA169715Can the ATV21/ATV212 VIA be setup for 0-10V speed and terminal control for start/stop?

Results 1 - 10 of 100