FAQs

FAQ Search
Most Recently Published FAQs

Results 91 - 100 of 100

FAQ ID Description
FA149423Was there a design change in the door operation on the HU365R Safety Switches?
Yes in 2009 there was a design change to the HU365R safety switches, making the door operation from top hinged to becoming side hinged on the left...
FA149425What is the differences between the EZM31200GCBU and EZM31200GCBE Main devices?
The EZM31200GCBU is a Underground ONLY feed, non-EUSERC, that comes standard with lugs. The EZM31200GCBE is a Underground ONLY feed, meets the EUSERC...
FA149424What main breaker is used in the EZM31600JCBC and does the main breaker have an adjustable trip?
The EZM31600JCBC includes a RJF36160U31A breaker and this breaker does have an adjustable Long time and Instantaneous settings. CTA-ID : 2060284
FA127070Does Square D manufacture 15KV C/T`s?
No ,these are not offered anymore . Try Trench Ltd. ( formerly Haefly Trench) in Canada or ITI - Instrument Transformer Inc. in FL .     CTA-ID...
FA148759Can Powerpact H, J, L, M, P, R, and Q frame circuit breakers be backfed?
Per UL 489 paragraph 9.1.1.13 and NEMA AB3 paragraph 3.4, molded case circuit breakers are fully tested and UL Listed for reverse connection unless...
FA148760What is the lug wire range for an HLL36030M71?
Lug kit AL150HD takes (1) #14 - 3/0 Al or Cu conductors per phase. CTA-ID : 2060451
FA1487579007FA1: what grade is the stainless steel?
Material is #302 stainless. CTA-ID : 2060472
FA148763What is the Interrupting Rating for a FJ Type Breaker?
The interrupting ratings for the FJ 2 or 3 pole breaker, 15-100A is 100K at 240V and 65K at 480V. CTA-ID : 2060356
FA148766What is the suffix ``X`` on the Powerpact circuit breakers?
That digit in the catalog number is for the rating plug. Since this trip unit does not have a rating plug, we use an `X` as a place holder. CTA-ID...
FA148756Will the Kirk or Federal keylock for a Masterpact MP work on a Masterpact NW circuit breaker?
Yes, just order the new provision for the NW, cat.# S48542. CTA-ID : 2060471

Results 91 - 100 of 100