FAQs

FAQ Search
Most Recently Published FAQs

Results 41 - 50 of 100

FAQ ID Description
FA152209Will the LDN36400CU33X breaker sense through the 13th harmonics?
Micrologic trip units for the Powerpact H, J, and L frame breakers are true RMS sensing through the 13th harmonic. CTA-ID : 2060577
FA152210What is the part number for a closing plate for the 8538 Series K Nema 1, 3R/12 enclosure?
The closing Plate (for all round operators) is a 9001K51. CTA-ID : 2060396
FA152211What is the difference between an XCKJ20541H7 and XCKJ10541H7?
The XCKJ10541H7 is SPDT with, with positive opening contacts, 1 normally open and 1 normally closed contact and the XCKJ20541H7  is 2 SPDT with 2...
FA152212How can the AOC output terminal be set up as a logic output in an Altivar 31 drive?
In the IO menu, set AOIt to 0A and then set dO to the desired logic output function such as rUn, Drive Running.  The logic output state is 1 (24V)...
FA152213What class overload protection does the ATV312 drive provide?
Based on this setting the drive provides class 10 overload protection. You can set this overload parameter in the SEt menu under ITH which is based...
FA152214What is a good source of information for the ATV312 drive?
Most information can be found in the following documents: DIA2ED2090404EN is the catalog. BBV46391 is the installation manual. BBV46385 is the programming...
FA152215Does the ATV312 cooling fan run all the time?
No. The fan starts automatically when the drive controller is commanded to run (receives a run command and a speed reference). It stops a few seconds after...
FA152216What are the part numbers for ATV312 DIN Rail mounting kits?
There are 2 DIN rail mount kits to allow some of the smaller size Altivar 312 drives to be mounted to 35mm DIN rail. Use VW3A9804 for ATV312H018M2,...
FA152217Can the Altivar 312 drive be set up to start with a run command active or to restart without requiring the run command to be cycled in the event of a power outage?
Yes it can. If the drive is set for 2 wire control  In the IO menu, set tCC=2C and tCt=LEL.  The same logic will apply to the run reverse command. CTA-ID...
FA152218Can the LUB32 use the smaller (less than 12 amps) control units?
Yes, it can. CTA-ID : 2060456

Results 41 - 50 of 100