| FA158713 | What are the repair parts for a QO816L100S, Series G4, Load Center? Only the parts listed below are considered field replaceable.
Cover - 4055309002
Interior Assembly - QON816L100
Neutral Bonding Screw - 4028329750... |
| FA158712 | What are the repair parts for a QO148L125GF, Series G1, Load Center? Only the parts listed below are considered field replaceable.
Cover - 4055332001
Interior Assembly - 4055332950
Neutral Bonding Screw - 4028329750... |
| FA158719 | What are the repair parts for a QO816L100DTS, Series G3, Load Center? Only the parts listed below are considered field replaceable.
Cover - 4055345351
Interior Assembly - 4055328050
Neutral Bonding Screw - 4028329750... |
| FA158718 | What class of fuse will the EZM31200FST accept? It will accept 300Vac Class T fuses Only.
CTA-ID : 2060636 |
| FA158708 | What are the repair parts for a HU465AWK Series E5 Heavy Duty Safety Switch? The parts listed here are the only field replaceable parts.
Line base assembly - 40552-189-50 (4-required. Arc Suppressor Assembly is not included)
Line... |
| FA158711 | HU465AWK: What is the current series number being produced? For Catalog number: HU465AWK
Current series number being produced: E5
Beginning date: 3/2012
CTA-ID : 2060641 |
| FA158720 | What is the main circuit breaker used in the EZM11200JCBT? The main circuit breaker is catalog number is PJM36120U31A.
CTA-ID : 2060626 |
| FA158715 | What is the main circuit breaker used in the EZM11200GCBT? The main circuit breaker is catalog number is PGM36120U31A.
CTA-ID : 2060625 |
| FA158717 | What main circuit breaker is used in the EZM31600JCBC? The main circuit breaker catalog numbers is RJF36160U31A
CTA-ID : 2060624 |
| FA158705 | What main circuit breaker is used in EZM11600GCBC? The main circuit breaker catalog numbers is RGF36160U31A
CTA-ID : 2060623 |