| FA170844 | Where can I find the manufacturing quality assurance procedure for the Altivar 61 and ATV71 drives? |
| FA166724 | What is the rated capacity of NQ panel copper bus? Bussing is UL listed for conductivity, at a minimum of 98%
CTA-ID : 2060391 |
| FA166688 | What degree of protection is the Altivar ATV18 unit? With the grey top on the unit it is rated IP31
WIth the grey top removed it is rated IP20
CTA-ID : 2062105 |
| FA165570 | Does the ATV312 have safe torque off? To be a true Safe Torque Off (STO) the drive must enable the implementation of applications up to safety Category 3 according to standard EN 954-1.... |
| FA165202 | What is the difference between Category 3 and Category 4 in reference to XCSDM safety interlocks? SIL2 is a Category 3 and SIL3 is a Category 4. SIL stands for `Systems Integrity Level` the higher the number the higher the safety standard.
CTA-ID... |
| FA164564 | What is the Nema rating of the S32598 extended handle for the L frame breaker? The S32598 handle can be marked Type 12, and it is in UL file E103955, volume 3, section 8.
CTA-ID : 2061429 |
| FA164399 | Are I line panels ABS rated? The I-Line panels meet American Bureau of Shipping Standards for steel vessels 2010 .
CTA-ID : 2058971 |
| FA164400 | Are NQ panels ABS rated? NQ panels meet American Bureau of Shipping Standards for steel vessels 2010 .
CTA-ID : 2058972 |
| FA164375 | Are the NF panelboards CSA rated? Yes, they have a CSA C22.2 rating.
CTA-ID : 2055041 |
| FA95564 | Are the FAL circuit breakers UL Listed? Yes, they are listed in file No. E10027 CTA-ID : 12364 |