FAQ Search

What is the catalog number for a Kirk Key Lock plus provisions for the Masterpact NW breaker?

Issue:
Selection of key interlock provisions for the Masterpact NW circuit breaker.

Product Line:
Masterpact NW

Environment:
Masterpact NW circuit breakers sold and supported in the USA.

Cause:
Procedure to select the correct provisions for a Kirk key interlock on a Masterpact circuit breaker.

Resolution:
S48923 is one Kirk Key lock for cradle locking
S48924 is two Kirk Key locks (keyed alike) for cradle locking
S48925 is two Kirk Key locks (keyed differently) for cradle locking
S48945 is one Kirk Key lock for circuit breaker locking
S48946 is two Kirk Key locks (keyed alike) plus provision for circuit breaker locking
S48947 is two Kirk Key locks (keyed differently) plus provision for circuit breaker locking

A lock order form must be submitted with the order. See 0613PL0001 for this order form. 

Link to catalog:

static.schneider-electric.us/docs/Circuit%20Protection/Masterpact%20Universal%20Power%20Circuit%20Breakers/IEC%20Rated%20Masterpact/0613PL0001.pdf

 
FA113119  |  12-Aug-2015  | Product Features
Bookmark Print
Please rate the content of this information
Unhelpful star.gif 1 star.gif 2 star.gif 3 star.gif 4 star.gif 5 Helpful
What can we do to improve this information?
Your email address