FAQ Search

Is there a lug kit for the bus bar on the Altstart ATS46?

No. Lugs should be selected to fit 0.55 inch or 14 mm holes based on the wire sizes used.
Lugs are not included with the soft starters.


CTA-ID : 7343
FA99511  |  14-Jan-2011  | Wiring
  • Please rate the content of this information
    Unhelpful 1 2 3 4 5 Helpful