FAQ Search

Can the Altistart units be obtained in special enclosures such as NEMA 3R, 4, 4X

We provide the ATS48 in NEMA 1, 12, or 3R enclosures as a standard offerring.  
Other enclosure types may be obtained through Seneca manufacturing on a case by case basis if requested.
Also, special enclosed soft starts may be obtained through the Industrial Applications Team ( IAT )
SquareD distributors can contact Seneca and/or IAT through their field offices.
IAT website contact is  (http://www.gsia.org/)


CTA-ID : 9866
FA99459  |  18-Jun-2012  | Product Features
  • Please rate the content of this information
    Unhelpful 1 2 3 4 5 Helpful