FAQ Search

If he has an over current trip on the breaker, what is the procedure for resetting it after a fault?
Motor operator reset procedure following trip after fault, with SDE. This procedure applies to the following breakers:
Compact NS up to 630 amps, NSF, NSJ
Powerpact C and D
Powerpact H, J and L

Mandatory manual reset following tripping due to an electrical fault (with over current trip switch): After clearing the fault, manually charge the charging handle until window says ``Charged``. Manually charging with the charging handle moves the breaker to open position from the tripped position, and resets the SDE. This can be done in the auto mode. It is not necessary to move switch to the manual mode. At this point the motor operator is ready for a remote closing command.


CTA-ID : 2060007
FA144776  |  14-May-2012  | Product Features
  • Please rate the content of this information
    Unhelpful 1 2 3 4 5 Helpful