Are the Zelio RSL Relays Din Rail Mountable?
Yes, it is din rail mountable on 1.38 in. (35 mm) DIN rail.
CTA-ID : 2059732
FA143720 |
09-Apr-2012
|
Product Features
PDF
Email
Bookmark
Print
Answers which others found helpful
> What is the catalog number of the Zelio Logic relay provided with the SR2PACKBD?
> Is there a DIN rail mount for a REG48PUN2LJLU temperature sensor?
> Can SRI Zelio relay be used with Din 3 din rail ?
Please rate the content of this information
Unhelpful
1
2
3
4
5
Helpful
What can we do to improve this information?
.
Your email address
> Submit Feedback > Cancel